imx8mq+yocto+4.9.51_ga:USB3.0 issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mq+yocto+4.9.51_ga:USB3.0 issue

1,174 Views
传策薛
Contributor V

Hi,community:

   

Our company has customized a motherboard for imx8mq, running yocto system, there are two usb3.0 interfaces on the motherboard, which are connected by two usb3.0hosts on the cpu, respectively connected to two usb3.0 interface cameras. At the same time, two cameras are taken to take the image stream, and the operation is normal at the beginning. After a period of time, the following error is printed:
[ 1163.760957] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.763187] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.765412] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.767643] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.769866] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.772090] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.774313] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.776538] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.778765] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.780990] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.783216] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.785440] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.787663] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1163.789894] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.792118] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.794342] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.796564] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.798786] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.801017] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1163.803243] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1163.805466] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1163.807692] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1163.809914] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.812142] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.814363] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1164.500502] systemd-journald[1737]: /dev/kmsg buffer overrun, some messages lost.
[ 1164.514332] xhci-hcd xhci-hcd.0.auto: Ring expansion failed

What is the problem with this?

Labels (1)
0 Kudos
3 Replies

751 Views
igorpadykov
NXP Employee
NXP Employee

Hi 传策 薛

RE: XHCI: Ring expansion failure — Linux USB 

please try latest Linux L4.14.78

linux-imx - i.MX Linux kernel 
Linux L4.14.78_1.0.0 Documentation
i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

751 Views
传策薛
Contributor V

Is Linux L4.14.78 a GA version?

pastedImage_1.png

0 Kudos

751 Views
igorpadykov
NXP Employee
NXP Employee

yes it is GA, one can check:

i.MX Software | NXP 

Best regards
igor

0 Kudos