imx8mp uuu emmc failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp uuu emmc failed

8,199 Views
HelloMather
Contributor I

hi nxp, 

         I am a fresher to imx8mp evk board, and i download yocto branch zeus to compile a version of uboot 2020.04 branch , but i find that i can not flash my emmc to bring my board up. the specific operation steps are as follows.

  • step1 ,sudo uuu -b emmc imx-boot-imx8mpevk-sd.bin-flash_evkxuzhu_0-1685623390625.pngxuzhu_0-1685623390625.png
  • step 2 , my serial port print info ,
  • U-Boot SPL 2020.04-5.4.70-2.3.0+ge42dee801e (May 25 2023 - 05:07:48 +0000)
    DDRINFO: start DRAM init
    DDRINFO: DRAM rate 4000MTS
    DDRINFO:ddrphy calibration done
    DDRINFO: ddrmix config done
    Normal Boot
    Trying to boot from BOOTROM
    Find FIT header 0x&480331a0, size 1031
    Need continue download 1024
    Download 3023360, total fit 3024992
    NOTICE: BL31: v2.2(release):rel_imx_5.4.70_2.3.0-0-gf1d7187f2
    NOTICE: BL31: Built : 05:33:04, May 25 2023


    U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e (May 25 2023 - 05:07:48 +0000)

    CPU: i.MX8MP[8] rev1.1 1600 MHz (running at 1200 MHz)
    CPU: Industrial temperature grade (-40C to 105C) at 34C
    Reset cause: POR
    Model: NXP i.MX8MPlus LPDDR4 EVK board
    DRAM: 6 GiB
    tcpc_init: Can't find device id=0x50
    setup_typec: tcpc port2 init failed, err=-19
    tcpc_init: Can't find device id=0x50
    setup_typec: tcpc port1 init failed, err=-19
    MMC: FSL_SDHC: 1, FSL_SDHC: 2
    [*]-Video Link 0Can't find cec device id=0x3c
    fail to probe panel device adv7535@3d
    fail to get display timings
    probe video device failed, ret -19

    [0] lcd-controller@32e80000, video
    [1] mipi_dsi@32e60000, video_bridge
    [2] adv7535@3d, panel
    Can't find cec device id=0x3c
    fail to probe panel device adv7535@3d
    fail to get display timings
    probe video device failed, ret -19
    In: serial
    Out: serial
    Err: serial

    BuildInfo:
    - ATF f1d7187
    - U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e

    MMC: no card present
    Detect USB boot. Will enter fastboot mode!
    Net:
    Error: ethernet@30be0000 address not set.

    Error: ethernet@30be0000 address not set.

    Error: ethernet@30bf0000 address not set.

    Error: ethernet@30bf0000 address not set.
    No ethernet found.

    Fastboot: Normal
    Boot from USB for mfgtools
    *** Warning - Use default environment for mfgtools
    , using default environment

    Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
    Hit any key to stop autoboot: 0

    ## Checking Image at 43800000 ...
    Unknown image format!
    Run fastboot ...
    USB init failed: -22
    u-boot=>

  • And My Questions is that uuu cmd not burn in my uboot compiled ? how can i burn the uboot into the emmc on my boards?
0 Kudos
Reply
6 Replies

8,177 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I hope you are doing well.

The logs show that you are on U-boot.

To flash it, I suggest use the next command:

uuu -b emmc_all <Your file name>.bin-flash_evk

But on your logs, I can see that you are on U-boot.

Best regards.

Jorge.

0 Kudos
Reply

8,163 Views
HelloMather
Contributor I

thank for your reply.

yes i just only want to flash uboot, but actually uuu just send it to ram memory and finally report usb_init failed -22.

is that any place need to be configured or modifyed?

do you encounter similar problems or any directional suggestions can  be given?

thank you so much.

0 Kudos
Reply

8,067 Views
HelloMather
Contributor I

thank you so much.

yes i get the same error as before. so i enable the DEBUG macro in boot source and capture the more detail message info as attachments.

the difference between your print and mine are mainly:

......

switch to partitions #0, OK
mmc2(part 0) is current device
flash target is MMC:2
Net: eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0

......

 

and mine are:

....

Command failed, result=1
Run fastboot ...
USB init failed: -22
Command failed, result=1

.......

 

could you help me analyze the reason for this difference?

 

 

 

0 Kudos
Reply

8,063 Views
HelloMather
Contributor I

here is my test bin

0 Kudos
Reply

8,139 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

It is not needed to modify, using the command on my last post should be enough. 

If you want to try, you can flash U-boot with the next command and attached files:

uuu -b emmc_all flash.bin u-boot.bin   

But I think you will get the same result, also I will attach the log that I got.

Best regards.

Jorge.

0 Kudos
Reply

8,023 Views
smithcoba
Contributor III

 

NXP Jorge7u7, 

uuu -b emmc_all flash.bin u-boot.bin

It seems the build-in script will flash the u-boot to the use partition at offset 0. 

and burn flash.bin to the boot1 emmc boot partition.

 

And the i.MX8MP bootloader is not u-boot only, it is combined by aft, ddr firmware, u-boot with checksum to make sure its integration. 

It seems could not direction replace the u-boot in flash.bin, which is wrapped by imx-mkimage, because of the crc. 

To speak frankly, NXP Jorge7u7, your command is totally wrong. And the understanding of i.MX8MP bootloader(flash.bin) is totally wrong. 

But it is very basic knowledge for you NXP tech support.


uuu -bshow emmc_all
uuu_version 1.4.149

.......

.......

FB: flash -raw2sparse all _image
FB: flash -scanterm -scanlimited 0x800000 bootloader _flash.bin

..........

 

0 Kudos
Reply