imx8mp | encoding two camera in parallel at 1080p

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp | encoding two camera in parallel at 1080p

Jump to solution
1,773 Views
shai_b
Senior Contributor II

Hello team,

I would like to know if our IMX8MPLUS could support capturing two cameras in parallel and being able to encode at 1080p60 (H.265/ H.264)?

Waiting for your kind feedback, Thanks.

Regards,

Shai

 

0 Kudos
Reply
1 Solution
3 Replies
1,758 Views
shai_b
Senior Contributor II

Hi @khang_letruong , Thanks.

I need the ability to compress (H.265) the two-camera video simultaneously can you please advise if the encoder could able to do that?

Waiting for your kind feedback, Many thanks.

KR,

Shai

0 Kudos
Reply
1,743 Views
khang_letruong
Senior Contributor III
0 Kudos
Reply
1,767 Views
khang_letruong
Senior Contributor III

Hi @shai_b ,

For our stereo camera, I was able to stream dual encoded video of the 2 sensors simultaneously. Our sensors are 1440x1080, not far from 1080p so I think it is ok.

Regards,

Khang