imx8mp | encoding two camera in parallel at 1080p

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mp | encoding two camera in parallel at 1080p

ソリューションへジャンプ
3,207件の閲覧回数
shai_b
Senior Contributor II

Hello team,

I would like to know if our IMX8MPLUS could support capturing two cameras in parallel and being able to encode at 1080p60 (H.265/ H.264)?

Waiting for your kind feedback, Thanks.

Regards,

Shai

 

ラベル(2)
0 件の賞賛
返信
1 解決策
3,176件の閲覧回数
khang_letruong
Senior Contributor III
0 件の賞賛
返信
3 返答(返信)
3,192件の閲覧回数
shai_b
Senior Contributor II

Hi @khang_letruong , Thanks.

I need the ability to compress (H.265) the two-camera video simultaneously can you please advise if the encoder could able to do that?

Waiting for your kind feedback, Many thanks.

KR,

Shai

0 件の賞賛
返信
3,177件の閲覧回数
khang_letruong
Senior Contributor III
0 件の賞賛
返信
3,201件の閲覧回数
khang_letruong
Senior Contributor III

Hi @shai_b ,

For our stereo camera, I was able to stream dual encoded video of the 2 sensors simultaneously. Our sensors are 1440x1080, not far from 1080p so I think it is ok.

Regards,

Khang