imx8mp Problems running M7 sound card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx8mp Problems running M7 sound card

跳至解决方案
4,153 次查看
aber
Contributor III

Hello nxp

    I run the M7 program on the development board refer to IMX_LINUX_USERS_GUIDE.pdf .

kernel version Linux imx8mpevk 5.15.32-lts

aber_0-1663055435870.png

After entering the system, I also copied asound.conf_rpmsg_imx8mp. After restarting, the system cannot find wm8960 audio. tried the 5.10.72 kernel version and couldn't find it either. Is this your bug? What needs to be corrected. thanks

aber_1-1663055551157.png

 

 

0 项奖励
回复
1 解答
4,138 次查看
aber
Contributor III

Hello AldoG 

     By default, M7 runs the helloworld program, and the debug serial port can output hello world. It seems that there is no problem, and the environment variables are also saved to ensure that it can run every boot.

在原帖中查看解决方案

0 项奖励
回复
8 回复数
4,140 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Did you save the environmental variables, when you set both the device tree and the script to fatload the M7 image?
Also, do you see anything in the M7 console?

Best regards,
Aldo.

0 项奖励
回复
4,103 次查看
aber
Contributor III

Hi AldoG 

    found the problem, dts needs to configure imx8mp-evk-rpmsg-lpv.dtb, bin cannot run hello_world, and the sound card can be found under the system. TKS!

0 项奖励
回复
4,119 次查看
aber
Contributor III

Hi AldoG 

    

NXP i.MX Release Distro 5.15-kirkstone imx8mpevk ttymxc1

imx8mpevk login: root
root@imx8mpevk:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: btscoaudio [bt-sco-audio], device 0: 30c20000.sai-bt-sco-pcm-wb bt-sco-pcm-wb-0 [30c20000.sai-bt-sco-pcm-wb bt-sco-pcm-wb-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 1: audiohdmi [audio-hdmi], device 0: i.MX HDMI i2s-hifi-0 [i.MX HDMI i2s-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 2: imxaudioxcvr [imx-audio-xcvr], device 0: XCVR PCM snd-soc-dummy-dai-0 [XCVR PCM snd-soc-dummy-dai-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
root@imx8mpevk:~# cat /proc/asound/cards
0 [btscoaudio ]: simple-card - bt-sco-audio
bt-sco-audio
1 [audiohdmi ]: audio-hdmi - audio-hdmi
audio-hdmi
2 [imxaudioxcvr ]: imx-audio-xcvr - imx-audio-xcvr
imx-audio-xcvr

Can't find wm8960 sound card.Do you have any good suggestions?

0 项奖励
回复
4,111 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hi,

I'll double check on my side as well, but please note that Cortex-M7 should be running imx8mp_m7_TCM_low_power_voice.bin or imx8mp_m7_TCM_low_power_wakeword.bin not the hello world.

Regarding WM8960 sound card, please note that RPMSG based dts have access to the codec trough I2C rpbus:
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk-r...

So make sure that you're running the correct Cortex-M7 application.

Best regards,
Aldo.

0 项奖励
回复
4,081 次查看
aber
Contributor III

Hi AldoG,

    I wonder why running other M7 .bin files why audio can't be found.

标记 (1)
0 项奖励
回复
4,069 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

This is because when using RPMSG based dts, it will probe the WM8960 sound card trough I2C RPBUS, this will need for Cortex-M7 application to have I2C enabled.

One could check the sai_low_power_audio SDK example for this.

Best regards,
Aldo.

0 项奖励
回复
4,107 次查看
aber
Contributor III

Hi AldoG

    I don't see these two files in the default bsp package  imx8mp_m7_TCM_low_power_voice.bin or imx8mp_m7_TCM_low_power_wakeword.bin 

   I have tried all these bins and can't find the sound card。

aber_0-1663726354577.png

 

0 项奖励
回复
4,139 次查看
aber
Contributor III

Hello AldoG 

     By default, M7 runs the helloworld program, and the debug serial port can output hello world. It seems that there is no problem, and the environment variables are also saved to ensure that it can run every boot.

0 项奖励
回复