imx8mp GStreamer without sprop-parameter-sets parameter

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mp GStreamer without sprop-parameter-sets parameter

1,700 次查看
zohargolan
Contributor III

Hi All,

I have a problem streaming from imx8mp AP to a simple RTP client.

The example in the i.MX 8 GStreamer User Guide section 10.1.5 is using the parameter sprop-parameter-sets as a key for the server and the client. This is working fine when I am streaming to VLC client. The problem is that the client, I need to connect too, does not have the provision to use the sprop-parameter-sets parameter.

The original server coomnad line is

gst-launch-1.0 -v filesrc location=FileName.mov ! qtdemux ! rtph264pay ! udpsink host=Client_IP port=5004

How can I modify this command to stream without the sprop-parameter-sets parameter?

 

Thank you

标记 (1)
0 项奖励
回复
1 回复

1,686 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

I think the following Community document would be of help on what you're trying to achieve:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Audio-Video-trough-Camera-stream-and-gst...

Best regards,
Aldo.
 

0 项奖励
回复