imx8mm wifi input password cannot connect, but you can connect to a router that does not require a p

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mm wifi input password cannot connect, but you can connect to a router that does not require a p

Jump to solution
2,375 Views
yzg
Contributor I

Hi,nxp

wifi input password cannot connect, but you can connect to a router that does not require a password

企业微信截图_16982327551353.png

企业微信截图_16982328371555.png

  

0 Kudos
Reply
1 Solution
2,213 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @yzg

Unfortunately, that WIFI module is unsupported for BSPs higher than 5.4.47.
I suggest you use this BSP or try a workaround described on the following link:

Enabling QCA9377 Wifi Driver for imx8mm-lpddr4-evk - NXP Community

I hope this information will be helpful.

Have a great day!

View solution in original post

0 Kudos
Reply
7 Replies
2,348 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @yzg

Could you please tell me your BSP version to review this issue?

 

0 Kudos
Reply
2,318 Views
yzg
Contributor I
kernel 5.15.71
0 Kudos
Reply
2,293 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @yzg

I tried using the BSP version LF5.15.71_2.2.2 and WIFI is working fine using a network with password and network without password. 

Are you trying using The Linux User's Guide connectivity section to properly set the WiFi?

i.MX Linux User's Guide (nxp.com)

0 Kudos
Reply
2,259 Views
yzg
Contributor I
Is wifi related to the configuration in uboot? I use LF_V202.04, ddr4 2g, 100% connection failure, but there are some small probability of uboot connection failure
0 Kudos
Reply
2,236 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @yzg

I don't think the problem could be related to Uboot configuration.
Are you using a custom board?
If not, what is your EVK version?
I would like to identify the WIFI module.

0 Kudos
Reply
2,225 Views
yzg
Contributor I
Hi,nxp
WIFI module is qca9377
0 Kudos
Reply
2,214 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @yzg

Unfortunately, that WIFI module is unsupported for BSPs higher than 5.4.47.
I suggest you use this BSP or try a workaround described on the following link:

Enabling QCA9377 Wifi Driver for imx8mm-lpddr4-evk - NXP Community

I hope this information will be helpful.

Have a great day!

0 Kudos
Reply