imx8m plus camera input resolution not changing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8m plus camera input resolution not changing

1,919 次查看
dennis3
Contributor V

On our previous processor (imx8m quad), our camera driver received v4l2 ioctl commands (via <dev>_s_parm) to set the desired video mode with the V4L2_BUF_TYPE_VIDEO_CAPTURE ioctl.  The driver would pass in parm.capture.capturemode that was one of the modes reported earlier in get enum_framesizes ioctl.

Our driver v4l2 subdev driver hasn't changed much between the two different kernels. Now, on the imx8m plus, it looks like the capture ioctl never get called though.  Instead. we get an <dev>_s_stream command but then the sensor is always left in the same default state for it's resolution.  The output resolution looks to be being scaled by the ISI layer instead.  For example, if I select via the camera api to stream 640x480, I'll see something like this in the dmesg output:

mxc-isi 32e00000.isi: input_size(2880,2016), output_size(640,480)

So it appears I'm missing something on how to configure in the HAL or driver layer that will allow the driver to change the capture size from the image sensor.  Any hints where this might be?  

 

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,909 次查看
joanxie
NXP TechSupport
NXP TechSupport

if you want to use v4l2 ctrl to change the resolution, you can try to use "v4l2-ctl -d /dev/video0 --verbose --set-fmt-video=width=xx,height=xx"

for ISI drivers, pls find the source code

"https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/staging/media/imx/imx8-isi-cap.c?h..."

 

0 项奖励
回复

1,902 次查看
dennis3
Contributor V

Thanks @joanxie 

So we're using Android and don't have the v4l2 controls.  Are you saying if we wish this functionality I need to modify the driver?

0 项奖励
回复

1,891 次查看
joanxie
NXP TechSupport
NXP TechSupport

android share the same linux kernel, you can find frame size setting in the  ISI driver as below:

"https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/staging/media/imx/imx8-isi-cap.c?h..."

 

0 项奖励
回复