imx8m plus camera input resolution not changing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8m plus camera input resolution not changing

1,916件の閲覧回数
dennis3
Contributor V

On our previous processor (imx8m quad), our camera driver received v4l2 ioctl commands (via <dev>_s_parm) to set the desired video mode with the V4L2_BUF_TYPE_VIDEO_CAPTURE ioctl.  The driver would pass in parm.capture.capturemode that was one of the modes reported earlier in get enum_framesizes ioctl.

Our driver v4l2 subdev driver hasn't changed much between the two different kernels. Now, on the imx8m plus, it looks like the capture ioctl never get called though.  Instead. we get an <dev>_s_stream command but then the sensor is always left in the same default state for it's resolution.  The output resolution looks to be being scaled by the ISI layer instead.  For example, if I select via the camera api to stream 640x480, I'll see something like this in the dmesg output:

mxc-isi 32e00000.isi: input_size(2880,2016), output_size(640,480)

So it appears I'm missing something on how to configure in the HAL or driver layer that will allow the driver to change the capture size from the image sensor.  Any hints where this might be?  

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,906件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

if you want to use v4l2 ctrl to change the resolution, you can try to use "v4l2-ctl -d /dev/video0 --verbose --set-fmt-video=width=xx,height=xx"

for ISI drivers, pls find the source code

"https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/staging/media/imx/imx8-isi-cap.c?h..."

 

0 件の賞賛
返信

1,899件の閲覧回数
dennis3
Contributor V

Thanks @joanxie 

So we're using Android and don't have the v4l2 controls.  Are you saying if we wish this functionality I need to modify the driver?

0 件の賞賛
返信

1,888件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

android share the same linux kernel, you can find frame size setting in the  ISI driver as below:

"https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/staging/media/imx/imx8-isi-cap.c?h..."

 

0 件の賞賛
返信