imx8m mini flash img error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8m mini flash img error

Jump to solution
3,055 Views
1269813285
Contributor I

I develop a custom board with imx8m mini ,when we execute the command

"sudo ./uuu_imx_android_flash.sh -f imx8mm -u ddr4 ",

the result is failed .it stop at the result

"3:13 1/ 1 [=================100%=================] SDP: boot -f u-boot-imx8mm-ddr4-evk-uuu.imx "

we doubt whether it is because of the ddr4 .

I noticed that the reference board using 2*16bit DDR4 for memory interface for 32bit data, and we used 1 bit DDR4 for memory for 16 bit data.
I wonder whether it is the cause of our problem.
Maybe we need to modify some code or configuration, Could you please give us some tips?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,004 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

I see that you have 2 threads about the same topic and got a response already from one of my colleagues, please take a look.

https://community.nxp.com/thread/533906

 

Best regards,

Aldo.

View solution in original post

0 Kudos
Reply
2 Replies
3,004 Views
1269813285
Contributor I

 we used 16 bit DDR4 for memory for 16 bit data.

0 Kudos
Reply
3,005 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

I see that you have 2 threads about the same topic and got a response already from one of my colleagues, please take a look.

https://community.nxp.com/thread/533906

 

Best regards,

Aldo.

0 Kudos
Reply