imx8m Yocto fsl-image-validation-imx vivante driver for X11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8m Yocto fsl-image-validation-imx vivante driver for X11

ソリューションへジャンプ
3,041件の閲覧回数
maciejka_miercz
Contributor II

Hello,

We have build Yocto for imx8m using a steps provided by the "i.MX Yocto project user guide" and after command xinit there isn't vivante drivers for the X11.

How to build vivatne drivers for X11?

ラベル(2)
0 件の賞賛
返信
1 解決策
2,461件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

I recommend reading the "i.MX Linux® Release Notes, Rev. L4.9.51_imx8mq-beta, 01/2018":

Page 5 / Features on i.MX 8MQuad:

No X11 backend supported in i.MX 8MQuad.

Regards,

Gary

元の投稿で解決策を見る

3 返答(返信)
2,461件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the document as below:

https://community.nxp.com/docs/DOC-330147?commentID=42866#comment-42866 

focus on the "6: Add GPU HW Acceleration for X11"

0 件の賞賛
返信
2,461件の閲覧回数
maciejka_miercz
Contributor II

Problem is that vivante drivers for i.mx8m are missing, they didn't exists in /usr/lib/xorg/modules/drivers/.

In Yocto there is recipe for xf86-video-imx-vivante but that driver is for the imx6 processor not imx8.

We bought imx8mqevk and we cannot test it in X11 enviroment. Our appliliance uses X11 to communicate with the user.

0 件の賞賛
返信
2,462件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

I recommend reading the "i.MX Linux® Release Notes, Rev. L4.9.51_imx8mq-beta, 01/2018":

Page 5 / Features on i.MX 8MQuad:

No X11 backend supported in i.MX 8MQuad.

Regards,

Gary