imx8m Yocto fsl-image-validation-imx vivante driver for X11

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8m Yocto fsl-image-validation-imx vivante driver for X11

Jump to solution
3,362 Views
maciejka_miercz
Contributor II

Hello,

We have build Yocto for imx8m using a steps provided by the "i.MX Yocto project user guide" and after command xinit there isn't vivante drivers for the X11.

How to build vivatne drivers for X11?

Labels (2)
0 Kudos
Reply
1 Solution
2,782 Views
gary_bisson
Senior Contributor III

Hi,

I recommend reading the "i.MX Linux® Release Notes, Rev. L4.9.51_imx8mq-beta, 01/2018":

Page 5 / Features on i.MX 8MQuad:

No X11 backend supported in i.MX 8MQuad.

Regards,

Gary

View solution in original post

3 Replies
2,782 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the document as below:

https://community.nxp.com/docs/DOC-330147?commentID=42866#comment-42866 

focus on the "6: Add GPU HW Acceleration for X11"

0 Kudos
Reply
2,782 Views
maciejka_miercz
Contributor II

Problem is that vivante drivers for i.mx8m are missing, they didn't exists in /usr/lib/xorg/modules/drivers/.

In Yocto there is recipe for xf86-video-imx-vivante but that driver is for the imx6 processor not imx8.

We bought imx8mqevk and we cannot test it in X11 enviroment. Our appliliance uses X11 to communicate with the user.

0 Kudos
Reply
2,783 Views
gary_bisson
Senior Contributor III

Hi,

I recommend reading the "i.MX Linux® Release Notes, Rev. L4.9.51_imx8mq-beta, 01/2018":

Page 5 / Features on i.MX 8MQuad:

No X11 backend supported in i.MX 8MQuad.

Regards,

Gary