imx8 mini soft reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8 mini soft reset

2,845 次查看
Ming
Contributor III

How do I issue a complete A53 core/M4 software reset within M4 code space? I attempted to assert reset bits in A53RCR0 and M4RCR registers but unsuccessful. 

0 项奖励
回复
4 回复数

2,806 次查看
b36401
NXP Employee
NXP Employee

The power cycle by PMIC is recommended instead of soft reset. In case of soft reset some modules may not to be resetted.

0 项奖励
回复

2,792 次查看
tom_orsi
Contributor I

Hello,

Thanks for the reply, can you provide a code snippet on how to completely reset both processors completely (A53, and M4) in software from the M4?

Thanks,

Tom

0 项奖励
回复

2,801 次查看
Ming
Contributor III

Should I trust watchdog reset then?

0 项奖励
回复

2,694 次查看
b36401
NXP Employee
NXP Employee

You you can do a reset using watchdog.

0 项奖励
回复