imx8 mini soft reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 mini soft reset

2,818 Views
Ming
Contributor III

How do I issue a complete A53 core/M4 software reset within M4 code space? I attempted to assert reset bits in A53RCR0 and M4RCR registers but unsuccessful. 

0 Kudos
Reply
4 Replies

2,779 Views
b36401
NXP Employee
NXP Employee

The power cycle by PMIC is recommended instead of soft reset. In case of soft reset some modules may not to be resetted.

0 Kudos
Reply

2,765 Views
tom_orsi
Contributor I

Hello,

Thanks for the reply, can you provide a code snippet on how to completely reset both processors completely (A53, and M4) in software from the M4?

Thanks,

Tom

0 Kudos
Reply

2,774 Views
Ming
Contributor III

Should I trust watchdog reset then?

0 Kudos
Reply

2,667 Views
b36401
NXP Employee
NXP Employee

You you can do a reset using watchdog.

0 Kudos
Reply