imx8 mini soft reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8 mini soft reset

2,819件の閲覧回数
Ming
Contributor III

How do I issue a complete A53 core/M4 software reset within M4 code space? I attempted to assert reset bits in A53RCR0 and M4RCR registers but unsuccessful. 

0 件の賞賛
返信
4 返答(返信)

2,780件の閲覧回数
b36401
NXP Employee
NXP Employee

The power cycle by PMIC is recommended instead of soft reset. In case of soft reset some modules may not to be resetted.

0 件の賞賛
返信

2,766件の閲覧回数
tom_orsi
Contributor I

Hello,

Thanks for the reply, can you provide a code snippet on how to completely reset both processors completely (A53, and M4) in software from the M4?

Thanks,

Tom

0 件の賞賛
返信

2,775件の閲覧回数
Ming
Contributor III

Should I trust watchdog reset then?

0 件の賞賛
返信

2,668件の閲覧回数
b36401
NXP Employee
NXP Employee

You you can do a reset using watchdog.

0 件の賞賛
返信