imx8 after kernel partition map size, booting is fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8 after kernel partition map size, booting is fail

763 次查看
sutton_kim
Contributor II

Hi 
I increase kernel partition map size 
for the kernel partitions, we use 4 kernel partition. 
two emergency kernel partition, two app kernel partition 
we use p6~p9 for the kernel . I increase 
I change 92160 to 115200 in 4 kernel partition . and I download to target board. 
but it occur error during booting. and it stops booting.

Error: can't get kernel image!

Please support me

Device        Boot    Start      End  Sectors  Size Id Type              
/dev/loop0p6          45150   137309    92160   45M 83 Linux.
-> change 
/dev/loop0p6          45150   160349   115200 56.3M 83 Linux

0 项奖励
回复
1 回复

707 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you use IMX8QM? what media do you use? emmc or sd card? could you share your uboot environment?

0 项奖励
回复