imx7d power up sequence issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx7d power up sequence issue

918件の閲覧回数
felixhsu
Contributor III

Hi All

Platform: i.MX7D with PF3000

Software: Linux 4.1.15.2.0.0

When power up the VLDO3V3 will have abnormal signal then pull high, why reason will bring abnormal signal?

How to fixed abnormal signal?

Thanks.

i.MX7D EVB

power up nxp evb.jpg

Customer board

power up svh.jpg

ラベル(3)
0 件の賞賛
返信
1 返信

755件の閲覧回数
art
NXP Employee
NXP Employee

There is nothing abnormal here. The small initial voltage on the VLDO3V3 power rail is most likely caused by some current back leakage somewhere in the hardware. It should not affect the hardware functionality.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信