imx7d flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx7d flash

2,923件の閲覧回数
aieenrezai
Contributor I

Dear Sir/Madam,

We want to used combine package of ram and nand flash such as: MT29TZZZ8D5JKETS-107 W.95Q or MT29TZZZ8D5JKEZB-107 W.95Q however they are not listed as supported device in NXP micron compatible list https://www.micron.com/~/media/documents/products/other-documents/nxp_compatibility_chart.pdf is using these devices straight forward? or I have to change parameters in the processor? how I have to change them? our processor is IMX7D

Apologize for copy, I attached the datasheets in this question.

Bests

タグ(2)
0 件の賞賛
返信
1 返信

2,752件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi aieen

according to documentation these parts have separate e.MMC and LPDDR3 interfaces,
which is JEDEC LPDDR3-compliant, so I believe they can be used with i.MX7D.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信