imx7d ENET1 not working with DP83825

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx7d ENET1 not working with DP83825

1,893 次查看
asmaa
Contributor V

Hello Everyone,

igorpadykov

I am working on enet1 on imx7d, interfacing it with DP83825. I have made the changes for PIN's as suggested in my last post. Here are my device tree changes

&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet1>;

clocks = <&clks IMX7D_ENET_AXI_ROOT_CLK>,
<&clks IMX7D_ENET_AXI_ROOT_CLK>,
<&clks IMX7D_ENET1_TIME_ROOT_CLK>,
<&clks IMX7D_PLL_ENET_MAIN_50M_CLK>;
clock-names = "ipg", "ahb", "ptp", "enet_clk_ref";
assigned-clocks = <&clks IMX7D_ENET1_TIME_ROOT_SRC>,
<&clks IMX7D_ENET1_TIME_ROOT_CLK>;
assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>;
assigned-clock-rates = <0>, <100000000>;
phy-mode = "rmii";
phy-handle = <&ethphy0>;
phy-supply = <&enet3v3>; /*Ethernet power enable*/
/delete-property/ fsl,magic-packet;
phy-reset-gpios = <&gpio3 26 GPIO_ACTIVE_HIGH>;
phy-reset-duration = <2>;
phy-reset-post-delay = <50>;
pinctrl-assert-gpios = <&gpio3 24 GPIO_ACTIVE_HIGH>;
status = "okay";

mdio {
#address-cells = <1>;
#size-cells = <0>;

ethphy0: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
//clock-names = "rmii-ref";
device-type = "ethernet-phy";
};
};
};

pinctrl_enet1: enet1grp {
fsl,pins = <
MX7D_PAD_ENET1_RGMII_TD0__ENET1_RGMII_TD0 0x73
MX7D_PAD_ENET1_RGMII_TD1__ENET1_RGMII_TD1 0x73
MX7D_PAD_ENET1_RGMII_TX_CTL__ENET1_RGMII_TX_CTL 0x73

MX7D_PAD_ENET1_RGMII_RD0__ENET1_RGMII_RD0 0x73
MX7D_PAD_ENET1_RGMII_RD1__ENET1_RGMII_RD1 0x73
MX7D_PAD_ENET1_RGMII_RXC__ENET1_RX_ER 0x73

MX7D_PAD_ENET1_TX_CLK__CCM_ENET_REF_CLK1 0x73
MX7D_PAD_EPDC_BDR0__CCM_ENET_REF_CLK2 (MX7D_PAD_SION | MX7D_PAD_CTL_DSE_X2)

MX7D_PAD_SD2_WP__ENET1_MDC 0x3
MX7D_PAD_SD2_CD_B__ENET1_MDIO 0x3

MX7D_PAD_ENET1_RGMII_RX_CTL__ENET1_RGMII_RX_CTL 0x73

MX7D_PAD_LCD_DATA21__GPIO3_IO26 (MX7D_PAD_CTL_PUS_100K_DOWN | MX7D_PAD_CTL_PUE | MX7D_PAD_CTL_SRE_SLOW | MX7D_PAD_CTL_DSE_X1) /* n_ENET_RST */
MX7D_PAD_LCD_DATA19__GPIO3_IO24 (MX7D_PAD_CTL_PUS_100K_DOWN | MX7D_PAD_CTL_PUE | MX7D_PAD_CTL_SRE_SLOW | MX7D_PAD_CTL_DSE_X1) /* n_ENET_PWDN */
>;
};

I am using an external clock from DP83825, the clock seems to be ok from DP83825. I have made the changes accordingly in mach-imx7d.c as follows:-

if (!IS_ERR(gpr)) {
        if (IS_ERR(enet_out_clk)) {
            pr_warn("%s: failed to get enet_out clock, assuming ext. clock source\n", __func__);
            /* use external clock for PHY */
            regmap_update_bits(gprIOMUXC_GPR1IMX7D_GPR1_ENET_TX_CLK_SEL_MASKIMX7D_GPR1_ENET_TX_CLK_SEL_MASK);
            regmap_update_bits(gprIOMUXC_GPR1IMX7D_GPR1_ENET_CLK_DIR_MASK0);
        } else {
            pr_warn("%s: found enet_out clock, assuming internal clock source\n", __func__);
            /* use internal clock generation and output it to PHY */
            regmap_update_bits(gprIOMUXC_GPR1IMX7D_GPR1_ENET_TX_CLK_SEL_MASK0);
            regmap_update_bits(gprIOMUXC_GPR1IMX7D_GPR1_ENET_CLK_DIR_MASKIMX7D_GPR1_ENET1_CLK_DIR_MASK);
            clk_put(enet_out_clk);

        }
    } else {
        pr_err("failed to find fsl,imx7d-iomux-gpr regmap\n");
    }

I went through this thread i.MX7 RMII 50MHz clock and found that for me as well ENET1_REF_CLK_ROOT is 0. Shall this bit be set or not, if using the external clock to ENET1?  Could you please provide some info on this, I am not clear after reading imx7d reference manual.

./memtool CCM.TARGET_ROOT78
SOC: i.MX7D
CCM Addr:0x30380000
CCM.TARGET_ROOT78 Addr:0x3038A700 Value:0x00000000 - See Target Interface for more information.

If it needs to be set while using the external clock as well, please suggest me how can I do it?

Other than this, am I missing anything to implement for ethernet?

Regards,

Asma

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,840 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Asma

what bsp used in the case, referenced  thread  issue should be fixed in last bsps.

Reference clock direction is defined by bit ENET1_TX_CLK_SEL,

register IOMUXC_GPR_GPR1 described in sect.8.2.4.2 GPR1 General

Purpose Register (IOMUXC_GPR_GPR1)

i.MX 7Dual Applications Processor Reference Manual

 In NXP i.MX7D Sabre uboot it is configured in function setup_fec()

mx7dsabresd.c\mx7dsabresd\freescale\board - uboot-imx - i.MX U-Boot 

RMII example can be found in imx7 colibri board

uboot-imx/colibri_imx7.h at imx_v2018.03_4.14.98_2.0.0_ga_var01 · varigit/uboot-imx · GitHub 

uboot-imx/colibri_imx7.c at imx_v2018.03_4.14.98_2.0.0_ga_var01 · varigit/uboot-imx · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,840 次查看
asmaa
Contributor V

I am using 4.19.35.

I checked IOMUXC.GPR_GPR1 register for ENET1_TX_CLK_SEL. It is set to 1. I think this is right.

pastedImage_1.png

0 项奖励
回复