imx7 ( warp7 ) partition via u-boot -urgent

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7 ( warp7 ) partition via u-boot -urgent

1,003 Views
edwardtyrrell
Senior Contributor I

Hi,

I have a totally blank ( new ) emmc on a custom imx7s board and am urgently trying to find a way to partition the emmc via u-boot. U-boot loads into ram fine and offers the following command which looks like it can do partitioning "mmc hwpartition [args...] - does hardware partitioning". I need to partition and set up boot areas to I can dd on to the virtual SD cards u-boot creates the normal way.

I have no mfgtool availability as fsl has stated that the bitbkake fsl-image-mfgtool-initramfs is not ready in Yocto Krogoth for the Warp7 board yet, hence why I'm not using it.

BR,

Ed.

Labels (3)
0 Kudos
Reply
1 Reply

746 Views
igorpadykov
NXP Employee
NXP Employee

Hi Edward

uboot emmc partitioning is not supported in nxp bsps, one can

post this to uboot mailing list, so that someone familiar with it could try to assist you.

U-Boot Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply