Fsl-Image-Gui does not give GUI upon HDMI connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fsl-Image-Gui does not give GUI upon HDMI connection

1,572 次查看
ajayvenkatakris
Contributor II

Hi,

    I have built the Fsl-image-gui with the help of the 10 step guide for the yocto project. The image is working but there are two problems, The board I have built the image for is the IMX6DL SABRE AUTO board.

1)Upon HDMI connection, I am getting the tty console rather than the GUI itself

I have altered the uboot parameters required for the HDMI connection 

setenv mmcargs=setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24

saveenv

2) If i connect the ethernet cable to the board, I am not able to access the internet and download using apt-get. Also it does not give a specific IPv4 Address. Previously I had tried using the MFG tool, and when I had connected the ethernet cable I was able to get internet access and I was getting an IPv4 address. What could be the reason for this? 

0 项奖励
回复
1 回复

1,297 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

1.

  Generally HDMI environment settings are described in the following thread.

HDMI Audio Setting 


  Offten problems relate to incorrect U-boot environment setting.

Below is useful link :

https://community.nxp.com/message/847843?commentID=847843#comment-847843 
 

  Also, please verify if HDMI is configured in kernel, using HDMI "Linux Menu Configuration Options",

described in "i.MX Linux® Reference Manual".

2.
 As for IP : please use dhclient (udhcpc) to get IP address.

Note : apt-get is not provided in our Yocto BSP.

apt-get not working 

https://community.nxp.com/message/806943?commentID=806943#comment-806943 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct
Answer button. Thank you!

0 项奖励
回复