imx6ull not booting after watchdog/core0 reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull not booting after watchdog/core0 reset

Jump to solution
7,730 Views
kevincronn
Contributor III

I have a bare metal application with the single core imx6ull. We are trying to get the chip to reset and boot from qspi flash after a watchdog reset but the imx6 does not come back up after reset. If we power cycle it will boot ok. I have tried to reset with the watchdog and by enabling the core0 reset in the SRC_SCR.

Watchdog reset code:

// force cold reset.
SRC->SCR &= ~SRC_SCR_WARM_RESET_ENABLE_MASK;

// enable clock in CCM
if(base == (WDOG_Type *)WDOG1_BASE)
{
CCM->CCGR3 |= 0x30000;
}
else if(base == (WDOG_Type *)WDOG2_BASE)
{
CCM->CCGR5 |= 0xC00;
}
else if(base == (WDOG_Type *)WDOG3_BASE)
{
CCM->CCGR6 |= 0x300000;
}
else
{
return;
}

base->WICR = WDOG_WICR_WICT(0x00) | WDOG_WICR_WIE(0);
base->WMCR = WDOG_WMCR_PDE(0);
base->WCR = WDOG_WCR_WDE_MASK; 

After writing the WDOG_WCR_WDE_MASK the system halts but never comes back.

Core0 code:

SRC->SCR |= 0xa0000;

Again after writing the core0 reset bit the system halts but never comes back.

Any help is appreciated.

Labels (2)
0 Kudos
Reply
1 Solution
7,596 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

recommended to remove power to the qspi as part of the processor reset, as it is done

in i.MX6ULL EVK schematic SPF-29364 signal nWDOG p.7, U708 p.10 :

MCIMX6ULL-EVK_DESIGNFILES

Design files, including hardware schematics, Gerbers, and OrCAD files.

Such solution places qspi to necessary state to support a reboot.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
2 Replies
7,596 Views
kevincronn
Contributor III

Thank you Igor, we are evaluating changing our hardware design.

0 Kudos
Reply
7,597 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

recommended to remove power to the qspi as part of the processor reset, as it is done

in i.MX6ULL EVK schematic SPF-29364 signal nWDOG p.7, U708 p.10 :

MCIMX6ULL-EVK_DESIGNFILES

Design files, including hardware schematics, Gerbers, and OrCAD files.

Such solution places qspi to necessary state to support a reboot.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 Kudos
Reply