I have a bare metal application with the single core imx6ull. We are trying to get the chip to reset and boot from qspi flash after a watchdog reset but the imx6 does not come back up after reset. If we power cycle it will boot ok. I have tried to reset with the watchdog and by enabling the core0 reset in the SRC_SCR.
Watchdog reset code:
// force cold reset.
SRC->SCR &= ~SRC_SCR_WARM_RESET_ENABLE_MASK;
// enable clock in CCM
if(base == (WDOG_Type *)WDOG1_BASE)
{
CCM->CCGR3 |= 0x30000;
}
else if(base == (WDOG_Type *)WDOG2_BASE)
{
CCM->CCGR5 |= 0xC00;
}
else if(base == (WDOG_Type *)WDOG3_BASE)
{
CCM->CCGR6 |= 0x300000;
}
else
{
return;
}
base->WICR = WDOG_WICR_WICT(0x00) | WDOG_WICR_WIE(0);
base->WMCR = WDOG_WMCR_PDE(0);
base->WCR = WDOG_WCR_WDE_MASK;
After writing the WDOG_WCR_WDE_MASK the system halts but never comes back.
Core0 code:
SRC->SCR |= 0xa0000;
Again after writing the core0 reset bit the system halts but never comes back.
Any help is appreciated.
解決済! 解決策の投稿を見る。
Hi Kevin
recommended to remove power to the qspi as part of the processor reset, as it is done
in i.MX6ULL EVK schematic SPF-29364 signal nWDOG p.7, U708 p.10 :
MCIMX6ULL-EVK_DESIGNFILES
Such solution places qspi to necessary state to support a reboot.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Igor, we are evaluating changing our hardware design.
Hi Kevin
recommended to remove power to the qspi as part of the processor reset, as it is done
in i.MX6ULL EVK schematic SPF-29364 signal nWDOG p.7, U708 p.10 :
MCIMX6ULL-EVK_DESIGNFILES
Such solution places qspi to necessary state to support a reboot.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------