imx6ull in linux4.1.15 : make cs drop to low level for all the time of 64 bytes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull in linux4.1.15 : make cs drop to low level for all the time of 64 bytes

577 Views
bighero77
Contributor III

my chip is imx6ull, the linux is linux 4.1.15
how to set the register to make cs keep drop durate several bytes?

now, my spi cs would drop every byte.

cs--_________-----  just send out 8 bit .
I need to send out 64 byte data in one cs drop:

cs--______________-- send out 64 byte .

what shall I do?

thanks.

Labels (3)
Tags (2)
0 Kudos
Reply
2 Replies

546 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @bighero77 

You can refer the spidev_test code to change the bits per word.

B.R

0 Kudos
Reply

559 Views
bighero77
Contributor III

csdrop.bmp

0 Kudos
Reply