my board is imx6ull. linux is linux4.1.15.
about one month ago. the waveform of CS is like this:
drop to low level during the whole burst (spi.message.length = 240). only 240byte data is transfered, the cs rise.
but, after one month. the module driver is not changed.
I find the cs would not transfer one burst (just one byte) and then it rise to high level.
both waveform are captured by spi.message.length = 240. every test, I would transfer 240 byte as one burst.
I really donnot know what register parameters would cause this difference.
would you please tell me what would control the cs drop pattern?
thanks a lot.
Hi @bighero77
Actually, when you use the SPI native PIN for CS signal line will like below picture:
When you use the GPIO for SPI cs pin, The cs pin signal line like this picture:
But it very strange you did nothing change, just one month later. Please double check if anyone change your dts file. Also please share me your dts file.
B.R
absolutely , I did not change anything.
would you please give one standard setting?
both in dts and module driver code?
thanks.