imx6ull cannot jtag debugging in emmc startup mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ull cannot jtag debugging in emmc startup mode

ソリューションへジャンプ
1,690件の閲覧回数
debugall
Contributor I

imx6ull cannot jtag debugging in emmc startup mode,jtag show Device "MCIMX6Y2" selected. Connecting to target via JTAG ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. Cannot connect to target. but Serial Downloader mode can jtag debug why?

0 件の賞賛
返信
1 解決策
1,680件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

if processor is running some code jtag connection may fail,

for reliable jtag connection recommended "Serial Downloader mode".

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,682件の閲覧回数
debugall
Contributor I

Pull down a 10k resistor,

but why is Serial Downloader mode ok

0 件の賞賛
返信
1,681件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

if processor is running some code jtag connection may fail,

for reliable jtag connection recommended "Serial Downloader mode".

 

Best regards
igor

0 件の賞賛
返信
1,685件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi debugall

 

for "total IR len" issue one can check if jtag_mode is grounded, as in i.MX6ULL EVK

schematic 

Design files, including hardware schematics, Gerbers, and OrCAD files

 

Best regards
igor

0 件の賞賛
返信