imx6ull cannot jtag debugging in emmc startup mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull cannot jtag debugging in emmc startup mode

Jump to solution
2,521 Views
debugall
Contributor I

imx6ull cannot jtag debugging in emmc startup mode,jtag show Device "MCIMX6Y2" selected. Connecting to target via JTAG ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. Cannot connect to target. but Serial Downloader mode can jtag debug why?

0 Kudos
Reply
1 Solution
2,511 Views
igorpadykov
NXP Employee
NXP Employee

if processor is running some code jtag connection may fail,

for reliable jtag connection recommended "Serial Downloader mode".

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
2,513 Views
debugall
Contributor I

Pull down a 10k resistor,

but why is Serial Downloader mode ok

0 Kudos
Reply
2,512 Views
igorpadykov
NXP Employee
NXP Employee

if processor is running some code jtag connection may fail,

for reliable jtag connection recommended "Serial Downloader mode".

 

Best regards
igor

0 Kudos
Reply
2,516 Views
igorpadykov
NXP Employee
NXP Employee

Hi debugall

 

for "total IR len" issue one can check if jtag_mode is grounded, as in i.MX6ULL EVK

schematic 

Design files, including hardware schematics, Gerbers, and OrCAD files

 

Best regards
igor

0 Kudos
Reply