imx6ull cannot jtag debugging in emmc startup mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull cannot jtag debugging in emmc startup mode

911 Views
debugall
Contributor I
imx6ull cannot jtag debugging in emmc startup mode,jtag show Device "MCIMX6Y2" selected. Connecting to target via JTAG ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. Cannot connect to target. but Serial Downloader mode can jtag debug why?
0 Kudos
Reply
1 Reply

906 Views
b36401
NXP Employee
NXP Employee

You can use Serial Downloader mode as Igor suggested. For the details please refer to chapter 8.9 "Serial Downloader" of the Reference Manual.

0 Kudos
Reply