imx6ull cannot jtag debugging in emmc startup mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ull cannot jtag debugging in emmc startup mode

1,294件の閲覧回数
debugall
Contributor I
imx6ull cannot jtag debugging in emmc startup mode,jtag show Device "MCIMX6Y2" selected. Connecting to target via JTAG ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. Cannot connect to target. but Serial Downloader mode can jtag debug why?
0 件の賞賛
返信
1 返信

1,289件の閲覧回数
b36401
NXP Employee
NXP Employee

You can use Serial Downloader mode as Igor suggested. For the details please refer to chapter 8.9 "Serial Downloader" of the Reference Manual.

0 件の賞賛
返信