imx6sx linux image hard-float or soft-float

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6sx linux image hard-float or soft-float

1,957 Views
茂实丁
Contributor II

Hello everybody!

    I'm starting kernel compilation for imx6sxsabresd board.  Does anyone know the compile flags when using bitbake to make linux image?

     Is the linux kernel compiled under “softfp” ?

Best Regards  !

       Ding!

Labels (3)
Tags (1)
0 Kudos
Reply
2 Replies

1,821 Views
Yuri
NXP Employee
NXP Employee

Hello,

  please look at the following

L3.14.28_1.0.0 toolchain


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,821 Views
茂实丁
Contributor II

Thank you !:smileyhappy:

0 Kudos
Reply