L3.14.28_1.0.0 toolchain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

L3.14.28_1.0.0 toolchain

Jump to solution
2,155 Views
thchison
Contributor I

Hello everyone

     I am a newer to YOCTO project, I have installed L3.14.28_1.0.0 and build it successfully for mx6q_sabresd board according document "Freescale_Yocto_Project_User's_Guide.pdf". Then I installed the tool chain according to website:Yocto Training - HOME , but I have get some differences as following:

    As mentioned in document "i.MX_6_BSP_Porting_Guide.pdf", the tool chain is:

         /opt/poky/1.4.1/sysroots/i686-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-

    But in my environment:

         /opt/poky/1.7/sysroots/i686-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-

    It seems that in my environment, the tool chain is not hardware float version, is that right?

         If yes, can anyone tell me how to get a hardware float version tool chain from L3.14.28_1.0.0?

Labels (1)
0 Kudos
Reply
1 Solution
1,916 Views
Yuri
NXP Employee
NXP Employee

Hello,

  From "i.MX_Linux_Release_Notes.pdf" : 

"Supports the GCC 4.9.1 toolchain with the hardware floating point build".


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,917 Views
Yuri
NXP Employee
NXP Employee

Hello,

  From "i.MX_Linux_Release_Notes.pdf" : 

"Supports the GCC 4.9.1 toolchain with the hardware floating point build".


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply