imx6sx linux image hard-float or soft-float

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6sx linux image hard-float or soft-float

2,088件の閲覧回数
茂实丁
Contributor II

Hello everybody!

    I'm starting kernel compilation for imx6sxsabresd board.  Does anyone know the compile flags when using bitbake to make linux image?

     Is the linux kernel compiled under “softfp” ?

Best Regards  !

       Ding!

ラベル(3)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,952件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  please look at the following

L3.14.28_1.0.0 toolchain


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,952件の閲覧回数
茂实丁
Contributor II

Thank you !:smileyhappy:

0 件の賞賛
返信