imx6solo u-boot porting from nandflash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6solo u-boot porting from nandflash

1,396 Views
luchengxu
Contributor I

imx6solo u-boot porting from nandflash starting ,what need to modify the configuration,how to modify nand driver in the uboot source code?

Labels (2)
0 Kudos
Reply
1 Reply

1,265 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please refer to attached Porting Guide Chapter 1 Porting U-Boot,

no changes are needed for booting from nand, just use mfg tools (with script

mfgtool2-yocto-mx-sabreauto-nand.vbs) on below link for programming uboot to nand

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

patch for U-Boot that integrates NXP kobs utility into U-Boot:

https://patchwork.ozlabs.org/patch/637573/

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply