imx6s vs imx6q memory bandwidth difference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6s vs imx6q memory bandwidth difference

2,241 Views
denniedegroot
Contributor I

Hello,

Currently I am developing on 2 custom boards with a identical layout. The difference is the used processor.

One board has a iMX6S and the other board a iMX6Q processor. Both boards have the same DDR configuration so the chips (MT41K128M16JT-125:K) and layout (32-bit) are identical. The DDR on the boards are independently calibrated.

However when running "bw_mem" (part of lmbench) I get very different results as the table below shows.

The 'bzero' test for instance is 6x slower on the Quadcore then on the Solo.

CommandiMX6 SoloiMX6 Quadcore
bw_mem -P 1 -N 4 128M rd1417.691318.39
bw_mem -P 1 -N 4 128M wr467.34373.44
bw_mem -P 1 -N 4 128M rdwr486.82397.27
bw_mem -P 1 -N 4 128M cp460.50342.82
bw_mem -P 1 -N 4 128M fwr2178.06370.24
bw_mem -P 1 -N 4 128M frd1158.55622.61
bw_mem -P 1 -N 4 128M fcp768.31317.41
bw_mem -P 1 -N 4 128M bzero2175.32339.56
bw_mem -P 1 -N 4 128M bcopy770.06355.44

Does anyone know why there is such a big difference between the Solo and Quadcore with identical DDR configuration?

Labels (3)
Tags (1)
1 Reply

1,932 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dennie

one can use profile tool for memory bandwidth analysis

About MMDC Profiling Tool for i.MX6 

Also difference may be caused by different NIC-301 settings

described in Chapter 45 Network Interconnect Bus System (NIC-301)

i.MX6DQ Reference Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply