imx6quad device tree SS with ECSPI or with GPIO?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6quad device tree SS with ECSPI or with GPIO?

Jump to solution
1,359 Views
J_W
Contributor III

Hi,

I am attempting to activate the ECSPI on my imx6q and I am a bit confused about discrepancies between the Reference Manual and my provided device tree - particularly regarding setting up the slave select pin. It turns out that the device tree has set up the SS with a GPIO instead of the ECSPI_SS mux command, is there any particular reason for that?

The default device tree:

 

&ecspi1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_ecspi1>;
	fsl,spi-num-chipselects = <2>;
	cs-gpios = <
		&gpio2 30 GPIO_ACTIVE_HIGH
		&gpio3 19 GPIO_ACTIVE_HIGH
	>;
	status = "okay";

	spidev0: spi@0 {
		compatible = "spidev";
		reg = <0>;
		spi-max-frequency = <54000000>;
	};

	spidev1: spi@1 {
		compatible = "spidev";
		reg = <1>;
		spi-max-frequency = <54000000>;
	};
};

pinctrl_ecspi1: ecspi1grp {
		fsl,pins = <
			MX6QDL_PAD_EIM_D18__ECSPI1_MOSI		0x0b0b0
			MX6QDL_PAD_EIM_D17__ECSPI1_MISO		0x0b0b0
			MX6QDL_PAD_EIM_D16__ECSPI1_SCLK		0x0b0b0
			MX6QDL_PAD_GPIO_19__ECSPI1_RDY		0x0b0b0
			MX6QDL_PAD_EIM_EB2__GPIO2_IO30		0x0b0b0 /* SPI CS0 */
			MX6QDL_PAD_EIM_D19__GPIO3_IO19		0x0b0b0 /* SPI CS1 */
		>;
	};

 

Note that the SPI CS is set up as MX6QDL_PAD_EIM_EB2__GPIO2_IO30.

 

However, in the reference manual there is another option, namely MX6QDL_PAD_EIM_EB2__ECSPI1_SS0. Why is this not used in the default device tree? (imx6q-tx6q-1036.dtsi)

I would like to use the built in SS functionality of the ECSPI instead of doing it manually. I'm uncertain on how to edit the device tree, in particular the cs-gpios part, is that part even required if the pin is set up as ECSPI1_SS0?

I was thinking about changing it to

 

&ecspi1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_ecspi1>;
	fsl,spi-num-chipselects = <1>;
	status = "okay";

	spidev0: spi@0 {
		compatible = "spidev";
		reg = <0>;
		spi-max-frequency = <10000000>;
	};
};

    pinctrl_ecspi1: ecspi1grp {
		fsl,pins = <
			MX6QDL_PAD_EIM_D18__ECSPI1_MOSI		0x0b0b0
			MX6QDL_PAD_EIM_D17__ECSPI1_MISO		0x0b0b0
			MX6QDL_PAD_EIM_D16__ECSPI1_SCLK		0x0b0b0
			MX6QDL_PAD_GPIO_19__ECSPI1_RDY		0x0b0b0
			MX6QDL_PAD_EIM_EB2__ECSPI1_SS0 		0x0b0b0
		>;
	};

 

Or do I need to describe the SS pin somehow inside the ecspi1 block?

0 Kudos
Reply
1 Solution
1,342 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Before kernel 4.14, native chip select usage on spi-imx driver was not functional so GPIO implementation was used, from 4.14 kernel and later this has been fixed so it is safe to use native CS.

Best regards,
Aldo.

View solution in original post

0 Kudos
Reply
1 Reply
1,343 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Before kernel 4.14, native chip select usage on spi-imx driver was not functional so GPIO implementation was used, from 4.14 kernel and later this has been fixed so it is safe to use native CS.

Best regards,
Aldo.

0 Kudos
Reply