imx6quad device tree SS with ECSPI or with GPIO?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6quad device tree SS with ECSPI or with GPIO?

ソリューションへジャンプ
1,414件の閲覧回数
J_W
Contributor III

Hi,

I am attempting to activate the ECSPI on my imx6q and I am a bit confused about discrepancies between the Reference Manual and my provided device tree - particularly regarding setting up the slave select pin. It turns out that the device tree has set up the SS with a GPIO instead of the ECSPI_SS mux command, is there any particular reason for that?

The default device tree:

 

&ecspi1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_ecspi1>;
	fsl,spi-num-chipselects = <2>;
	cs-gpios = <
		&gpio2 30 GPIO_ACTIVE_HIGH
		&gpio3 19 GPIO_ACTIVE_HIGH
	>;
	status = "okay";

	spidev0: spi@0 {
		compatible = "spidev";
		reg = <0>;
		spi-max-frequency = <54000000>;
	};

	spidev1: spi@1 {
		compatible = "spidev";
		reg = <1>;
		spi-max-frequency = <54000000>;
	};
};

pinctrl_ecspi1: ecspi1grp {
		fsl,pins = <
			MX6QDL_PAD_EIM_D18__ECSPI1_MOSI		0x0b0b0
			MX6QDL_PAD_EIM_D17__ECSPI1_MISO		0x0b0b0
			MX6QDL_PAD_EIM_D16__ECSPI1_SCLK		0x0b0b0
			MX6QDL_PAD_GPIO_19__ECSPI1_RDY		0x0b0b0
			MX6QDL_PAD_EIM_EB2__GPIO2_IO30		0x0b0b0 /* SPI CS0 */
			MX6QDL_PAD_EIM_D19__GPIO3_IO19		0x0b0b0 /* SPI CS1 */
		>;
	};

 

Note that the SPI CS is set up as MX6QDL_PAD_EIM_EB2__GPIO2_IO30.

 

However, in the reference manual there is another option, namely MX6QDL_PAD_EIM_EB2__ECSPI1_SS0. Why is this not used in the default device tree? (imx6q-tx6q-1036.dtsi)

I would like to use the built in SS functionality of the ECSPI instead of doing it manually. I'm uncertain on how to edit the device tree, in particular the cs-gpios part, is that part even required if the pin is set up as ECSPI1_SS0?

I was thinking about changing it to

 

&ecspi1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_ecspi1>;
	fsl,spi-num-chipselects = <1>;
	status = "okay";

	spidev0: spi@0 {
		compatible = "spidev";
		reg = <0>;
		spi-max-frequency = <10000000>;
	};
};

    pinctrl_ecspi1: ecspi1grp {
		fsl,pins = <
			MX6QDL_PAD_EIM_D18__ECSPI1_MOSI		0x0b0b0
			MX6QDL_PAD_EIM_D17__ECSPI1_MISO		0x0b0b0
			MX6QDL_PAD_EIM_D16__ECSPI1_SCLK		0x0b0b0
			MX6QDL_PAD_GPIO_19__ECSPI1_RDY		0x0b0b0
			MX6QDL_PAD_EIM_EB2__ECSPI1_SS0 		0x0b0b0
		>;
	};

 

Or do I need to describe the SS pin somehow inside the ecspi1 block?

0 件の賞賛
返信
1 解決策
1,397件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Before kernel 4.14, native chip select usage on spi-imx driver was not functional so GPIO implementation was used, from 4.14 kernel and later this has been fixed so it is safe to use native CS.

Best regards,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,398件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Before kernel 4.14, native chip select usage on spi-imx driver was not functional so GPIO implementation was used, from 4.14 kernel and later this has been fixed so it is safe to use native CS.

Best regards,
Aldo.

0 件の賞賛
返信