imx6qdl time interval at SCLK.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6qdl time interval at SCLK.

跳至解决方案
2,045 次查看
dahyunkim
Contributor I

Hello, 

I had a problem in imx6qdl and I have to reduce the interval of the SCLK(spi clock).

Actually, I have to get no interval in spi clock like this.(Yello is SCLK)

pastedImage_1.png

But i.mx6qdl SCLK is like this.

pastedImage_2.png

There is 1us interval time. I use 4.5Mhz spi transfer speed.

I am wondering the way can modify the interval of the spi clock.

Do you know the way control of the spi clock?

Is the interval time related in Clock Controller Module? 

Thank you.

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
1,930 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dahyun

>I am wondering the way can modify the interval of the spi clock.

>Do you know the way control of the spi clock?

interval is caused by processor internal buses delays and can not be changed, sorry.

>Is the interval time related in Clock Controller Module? 

no

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,931 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dahyun

>I am wondering the way can modify the interval of the spi clock.

>Do you know the way control of the spi clock?

interval is caused by processor internal buses delays and can not be changed, sorry.

>Is the interval time related in Clock Controller Module? 

no

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复