IMX8M_how to write LPDDR4 MR26/MR33 mode register?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M_how to write LPDDR4 MR26/MR33 mode register?

1,258件の閲覧回数
alexjiang
Contributor II

IMX8M_how to write LPDDR4 MR26 mode register?

Platform: IMX8M + 4Gb 2channel 32bit LPDDR4;

1. We need to use LPDDR4 mode register: MR26/MR33(in JEDEC this MR26 is RFU),

    so we want to write a code to MR26/MR33,how to operate?

1> if IMX8M have register map to MR26/MR33, we can write the register address;

2> or if we can send the command: MRW  in uboot? how to operate?

0 件の賞賛
返信
1 返信

1,136件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alex

seems MR registers can be set using MRCTRL0/1 registers described in

sect.9.3.3.1.6/7 Mode Register Read/Write Control Register
i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

uboot lpddr4_mr_write() example

ddrphy_utils.c\imx8m\ddr\drivers - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信