imx6q ubuntu GPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q ubuntu GPU

3,054 Views
frankweng
Contributor III

yocto :L4.1.15.1.2

OS: ubuntu16.04 and 18.04

板子:imx6Q 

按照按照下面兩篇 poring GPU
https://community.nxp.com/thread/454418

https://community.nxp.com/docs/DOC-330147

都作到最後,run glmark2 Or 其他的Command 都會出現下面的問題
libGL error: driver exports no extensions (/usr/ lib/dri/ vivante_dri.so: undefined symbol: __driDriverExtensions)
libGL error: failed to load driver: vivante

使用的相關套件(大多是從yocto 的code中dowload 資料夾中抓來用) ,所有都是在imx6Q kit 上build code
firmware-imx-5.4
imx-vpu-5.4.33
imx-lib-5.4
libfslcodec-4.0.8(or imx-codec-4.0.9 )
imx-gpu-viv-5.0.11.p8.4-hfp(Or p8.3)
libimxvpuapi-0.10.3
gstreamer-imx-1.0
xserver-xorg-video-imx-viv-5.0.11.p8.4( Or p8.3 配合imx-gpu-viv的版本)

kernel module build 在一般的x86伺服器上build

有試過yocto 原本kernel 中的gpu-viv driver

也參考  https://boundarydevices.com/customizing-ubuntudebian-kernels/ 

buid過5.0.11.p7.4 /5.0.11.p8.6 /6.2.2.p0 

結果只有5.0.11.p8.6 可以看到畫面,其他都無法看到畫面

就算是5.0.11.p8.6 一樣會有下面的問題

 libGL error: driver exports no extensions (/usr/ lib/dri/ vivante_dri.so: undefined symbol: __driDriverExtensions)
libGL error: failed to load driver: vivante
能否協助,謝謝

Labels (2)
0 Kudos
Reply
1 Reply

2,816 Views
joanxie
NXP TechSupport
NXP TechSupport

maybe you can refer to the doc as below:

https://community.nxp.com/message/1023233 

0 Kudos
Reply