imx6q uboot logo problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q uboot logo problem

ソリューションへジャンプ
3,125件の閲覧回数
yuhundehao
Contributor III

I've patched the patch logo。

bsp:uboot2009 linux-3.0.35.

Such as the picture should be displayed in the red box on the left side of the show, now displayed on the right side of the display, which is what causes

pastedImage_3.jpg

ラベル(1)
0 件の賞賛
返信
1 解決策
2,885件の閲覧回数
yuhundehao
Contributor III

The problem has been solved for the following reasons:

<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=1 seek=6291456 skip=70">Write Log</CMD>

Skip patch requirements are 54, first changed to 70, up to the big demand。

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,886件の閲覧回数
yuhundehao
Contributor III

The problem has been solved for the following reasons:

<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=1 seek=6291456 skip=70">Write Log</CMD>

Skip patch requirements are 54, first changed to 70, up to the big demand。

0 件の賞賛
返信
2,885件の閲覧回数
yuhundehao
Contributor III

Do I have a problem with this  0001-Enable-uboot-logo-for-HDMI-LCD-and-LVDS.patch?

0 件の賞賛
返信
2,885件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

had you adjusted timings for custom lcd:

How to change SABRE-SD screen resolution in LOLLIPOP(5.0.0? 

0 件の賞賛
返信
2,885件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yuhundehao

please try uboot logo patches from

https://community.freescale.com/docs/DOC-98109 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信