[imx6q] frequency deviation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[imx6q] frequency deviation

11,218 Views
jackeyko
Contributor III

Hi NXP,

We changed 24MHz to 24.576MHz for audio clock.

But the frequency was actually 24.5745 MHz in CLKO1 . Please find the attahced file.

I would like to know why is 24.5745 MHz measured.

24.5745MHz to CLKO1 .PNG

Thanks,

Jackey

Labels (4)
2 Replies

11,148 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jackey

24.5745 MHz may be measured due to crystal accuracy and

temperature drift. In general frequency can be adjusted by tuning

loading capacitors.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

11,148 Views
jackeyko
Contributor III

Hi Igor,

Thanks for your message.

I will check the crystal accuracy and temperaure drift and adjust the loading capacitors.

Thanks,

Jackey

0 Kudos
Reply