imx6q, fall-back boot mode on errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q, fall-back boot mode on errors

1,795件の閲覧回数
angelo_d
Senior Contributor I

Hi, was wondering, is the OTG (serial loader) the only fall-back mode in case of any error booting ? I mean, on a corrupted app/bootloader boot (i.e. U-boot), whatever boot setting is set, does imx6 always fall back to serial loader (OTG) ?

Thanks

angelo

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,639件の閲覧回数
angelo_d
Senior Contributor I

Hi Igor, 

quite clear, many thanks.

0 件の賞賛
返信

1,639件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi angelo

yes in case of any error, boot ROM falls back to serial downloader as described

for example in sect.8.2.5 Internal Boot mode i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

"If an error occurs during the internal boot, the boot code jumps to the Serial Downloader"

For some processors there are differencies in behaviour, for example in

SD/MMC manufacture mode, [sect.8.11 SD/MMC manufacture mode i.MX6SDL Reference Manual ]

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf 

"When the internal boot and recover boot (if enabled) failed, the boot goes to the
SD/MMC manufacture mode before the serial download mode."

Note this is description for boot ROM, if processor executes custom bootloader this

may be not applicable.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------