imx6q ext4 file system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q ext4 file system

Jump to solution
3,745 Views
yilingxu
Contributor III

Hi, my rootfs is put in SD card, and is not packaged, specifically, there are /bin, /boot, /dev, /user ... in my second partition of SD card. The linux kernel can mount this rootfs and it works well.

Now I want to sign my rootfs, so I want to make the rootfs as an image. Specifically, I want to make the rootfs as imx-imx6qsabresd.ext4, and put imx-imx6qsabresd.ext4 in my second partition of SD card. How can linux kernel work with this type of rootfs?

I am new with rootfs, can anyone give me some suggestions? thanks a lot.

Yiling Xu

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,562 Views
jimmychan
NXP TechSupport
NXP TechSupport

Are you talking about copying the root file system?

Attached is the Linux User's guide. please refer to the 4.3.5. for more details.

View solution in original post

0 Kudos
Reply
1 Reply
3,563 Views
jimmychan
NXP TechSupport
NXP TechSupport

Are you talking about copying the root file system?

Attached is the Linux User's guide. please refer to the 4.3.5. for more details.

0 Kudos
Reply