imx6q ddr3 frequency setup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6q ddr3 frequency setup

跳至解决方案
1,404 次查看
wangcuixmwangcu
Contributor III

imx6q ddr3 frequency can be config to 400Mhz or 528Mhz. And can it be configed to 600Mhz or 800Mhz?

标签 (1)
0 项奖励
回复
1 解答
1,173 次查看
igorpadykov
NXP Employee
NXP Employee

Hi wangcuixm

not, as i.MX6Q MMDC max. operating frequency is 532MHz according to

i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,174 次查看
igorpadykov
NXP Employee
NXP Employee

Hi wangcuixm

not, as i.MX6Q MMDC max. operating frequency is 532MHz according to

i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复