imx6q ddr3 frequency setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q ddr3 frequency setup

ソリューションへジャンプ
1,275件の閲覧回数
wangcuixmwangcu
Contributor III

imx6q ddr3 frequency can be config to 400Mhz or 528Mhz. And can it be configed to 600Mhz or 800Mhz?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,044件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wangcuixm

not, as i.MX6Q MMDC max. operating frequency is 532MHz according to

i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,045件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wangcuixm

not, as i.MX6Q MMDC max. operating frequency is 532MHz according to

i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信