imx6q ddr3 frequency setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q ddr3 frequency setup

Jump to solution
1,403 Views
wangcuixmwangcu
Contributor III

imx6q ddr3 frequency can be config to 400Mhz or 528Mhz. And can it be configed to 600Mhz or 800Mhz?

Labels (1)
0 Kudos
Reply
1 Solution
1,172 Views
igorpadykov
NXP Employee
NXP Employee

Hi wangcuixm

not, as i.MX6Q MMDC max. operating frequency is 532MHz according to

i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,173 Views
igorpadykov
NXP Employee
NXP Employee

Hi wangcuixm

not, as i.MX6Q MMDC max. operating frequency is 532MHz according to

i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply