imx6q custom board can't enter the android6.0 system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q custom board can't enter the android6.0 system

1,017件の閲覧回数
kaneshi
Contributor I

my imx6q custorm board with 1GB DDR.After burning the compiled Android firmware, it has been repeatedly restarted in the Android logo after power-on. How to solve this problem?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

937件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kane

one can try to program image on flash using documentation Android M6.0.1_2.1.0 BSP Documentation

i.MX 6 Series Manufacturing Toolkit for Android M6.0.1_2.1.0 Release

If this will not help, run ddr test i.MX6/7 DDR Stress Test Tool V3.00 

and update image with new calibration coefficients found from test.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

937件の閲覧回数
kaneshi
Contributor I

hi igorpadykov

            the uboot and kernel is ok。The current problem is that my custom board can't enter the Android file system.

0 件の賞賛
返信