imx6q custom board can't enter the android6.0 system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q custom board can't enter the android6.0 system

569 Views
kaneshi
Contributor I

my imx6q custorm board with 1GB DDR.After burning the compiled Android firmware, it has been repeatedly restarted in the Android logo after power-on. How to solve this problem?

Labels (2)
0 Kudos
Reply
2 Replies

489 Views
igorpadykov
NXP Employee
NXP Employee

Hi kane

one can try to program image on flash using documentation Android M6.0.1_2.1.0 BSP Documentation

i.MX 6 Series Manufacturing Toolkit for Android M6.0.1_2.1.0 Release

If this will not help, run ddr test i.MX6/7 DDR Stress Test Tool V3.00 

and update image with new calibration coefficients found from test.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

489 Views
kaneshi
Contributor I

hi igorpadykov

            the uboot and kernel is ok。The current problem is that my custom board can't enter the Android file system.

0 Kudos
Reply