imx6q: building linux image with both fb & x11 backends

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q: building linux image with both fb & x11 backends

923件の閲覧回数
pj0585
Contributor III

Hi,

I want to build the latest fsl-community-bsp image

(fsl-L3.14.28_1.0.0_ga). I can choose to build any one backend (fb, x11,

wayland or directfb). The libraries of the other backends are removed

or not built.

Is it possible to build the image for framebuffer (fb) backend but

also include libraries of the x11 backend ? If yes, can someone please point out to me how can I do this?

Regards, Pj

ラベル(4)
タグ(3)
0 件の賞賛
返信
0 返答(返信)