imx6q MII RGMII

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q MII RGMII

2,752 Views
eliaz
Contributor II

Can the imx6q use RGMII & MII peripheries  in the same time (Can these peripheries be active in the same time)?

Labels (2)
0 Kudos
Reply
4 Replies

2,533 Views
eliaz
Contributor II

can you be more specific about multiplexing , which signal is shared between the interfaces?

0 Kudos
Reply

2,533 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

 IMX6Q has ENET module, which supports MII, RMII, RGMII interfaces

Pins affected are described in Table 23-1 (ENET External Signals) of

the i.MX6 RM (Rev. 3, 07/2015). Only single interface may be used

at a time because of multiplexing. 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 Kudos
Reply

2,533 Views
eliaz
Contributor II

can you be more specific about multiplexing , which signal is shared between the interfaces?

0 Kudos
Reply

2,533 Views
eliaz
Contributor II

can you be more specific about multiplexing , which signal is shared between the interfaces?

0 Kudos
Reply